Other Parts Discussed in Thread: LM62440-Q1, LM63460-Q1
LM61460-Q1 and LM62440-Q1 are use the same DIE ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM61460-Q1 and LM62440-Q1 are use the same DIE ?
Hi Jian,
There are effectively two pin differences here (RT and EN/SYNC become MODE/SYNC and EN) -- otherwise no difference in performance other that the current limit. You may also consider the LM63460-Q1 if you need 6A -- this is similar to the LM61460-Q1 but has a package with easier layout and with improved thermal performance.
Regards,
Tim