I have an EMI application where I need to use a linear regulator to generate 0.85V from a 5V input. This load is 2A continuous but may go to 3.5A for 500ms at initialization. So for heat dissipation, I need to consider 2A@4.2V or so. Can you confirm if this device can dissipate this kind of heat? The junction to case theta seems to be best for the bottom, so a heat sink on top will not help. Do you have recommendation for how to dissipate this much heat?
Thank you