This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524-Q1: recommend PMIC

Part Number: LP87524-Q1
Other Parts Discussed in Thread: LP8758, LP8752-Q1, TPS65266, TPS563900, TPS65400, TPS65265

Hi Sir,

My customer is looking for a 4-ch PMIC device and it could support the output power including 0.9V/2~3A, 3.3V/3A, 1.5V/1.5A, and 1.8V/ 1.5A.

Could I recommend the LP87524-Q1 to him? or have another device? A non-q grade device also is fine.

Due to the 4-ch PMIC device having high-cost issues, I also would like to find a 3-PMIC device for the customer, it can support the output power including 0.9V/2~3A, 3.3V/3A, 1.5V/1.5A. Could you please advise a device to me?