Hi. I am using pSpice Simulator for TI components. I downloaded the transient model provided from the LM3409 datasheet. This got me a base schematic to work with. I modified it to be how my circuit is. The only thing I am having trouble with is modeling an LED after the LEDS I am using: CREE XP-G3. I tried using modeling application as I saw you could model an LED there with the correct specs. With the current software I am using, It seems like this is not an option. So I am seeking help to find a work around or a way to model this LED so I can get this simulation going. I believe if TI support could model the LED and send it to me, I could load it into my schematic and it might work great. Other than that, I am hoping TI support can provide insight on how to work around this. I have seen using a diode and a voltage source to simulate an LED, but I have not had luck with that.
Here is the datasheet for the LED I am using.
https://assets.cree-led.com/a/ds/x/XLamp-XPG3.pdf
More specifically I am using the following LED: "Forward voltage (@2000mA, 85C) - white Typical Forward V = 3.06
Any help is appreciated.
Thank you.