Hello,
My customer has a LTO battery cell that they want to be able to discharge as low as possible. I have two questions:
- What gauge in our portfolio has the lowest VDD? This is not something that is sortable on the parametric table so it isn't easy to find.
- Do we have any gauges in our portfolio where you can separate the VDD of the gauge and the analog front end that measures the battery?
- This would allow a small boost converter, for example the TPS61099 which can run down to 0,7V to keep the gauge powered through a deeply discharged battery
Thanks!
John