This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24100: BQ24100 is damaged after several months in the field. >1% failure rate

Part Number: BQ24100

I am having the same issue.   Boards with BQ24100 return from the field with TS pin having low impendence to ground (100 ohms) or input to ground shorted AND output to ground shorted.    Did the post a couple years ago get resolved?   thx