Other Parts Discussed in Thread: PMP20042, , LM5175, TPS25858-Q1, TPS25772-Q1, TPS55288-Q1, TPS55288
Hi Team,
Our customer is going to design a 4 to 6 port USB-C charging station for vehicles with supply voltage of 12V from the battery. They prefer to have 60w power output per port but if not feasible 45w will do. He is considering a PD system and looking at TPS25851-Q1 since it already includes the DC/DC converter. Since the power is coming from a 12V battery, does he need to add a boost converter such as LM5175 which is used in the PMP20042 reference design to power the TPS25851-Q1?
Due to the limitation of their soldering equipment, they preferred package that can be soldered using hot air. Is the TPS25858-Q1 a suitable device?
Since the total system power is 60W x 6 ports = 360W and there are 6 ports, he will need 360W, 12V to 20V boost converter and 3 units of TPS25858-Q1. Is this correct? Do we have a simpler solution?
Regards,
Danilo