After programming a golden gauge file, I run three charge discharge cycles on the single cell 21700 battery in application
The Design capacity is 3600mAh
The termination voltage in golden gauge file is set to 3150mV, Residual capacity is 100mAhours .
For the First guage correctly guages the SOC and sets it to 0% when voltage is close to 3200mV. On the second and third cycles, the voltage at which SOC is set to 0% drifts upwards to 3300mV and 3450mV respectively. THis is affecting run time of device.
I expect the end voltage to be ~3200mV due to the termination voltage setting in the battery.
THe discharge load is constant power of approximately 1.6W. Charging current is 1A.
What could be causing this drift?