Hi,
We are considering replacing the TLV431BIDCKR (-40°C to 85°C) with the TLV431BQDCKR (-40°C to 125°C).
If I use the TLV431BQDCKR from -40°C to 85°C, are the parameters in the datasheet specs for the TLV431BIDCKR the same?
Thanks,
Astro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are considering replacing the TLV431BIDCKR (-40°C to 85°C) with the TLV431BQDCKR (-40°C to 125°C).
If I use the TLV431BQDCKR from -40°C to 85°C, are the parameters in the datasheet specs for the TLV431BIDCKR the same?
Thanks,
Astro
Hello Astro,
That is correct.
Thanks.