Hello,
What are the differences among LP875610RNFRQ1, LP87561IRNFRQ1 and LP87561IRNFRQ1?
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What are the differences among LP875610RNFRQ1, LP87561IRNFRQ1 and LP87561IRNFRQ1?
Best regards,
K.Hirano
Hello,
Let me correct my question here.
What are the differences among LP875610RNFRQ1, LP87561IRNFRQ1 and P87561IRNFRQ1?
Best regards,
K.Hirano
Hi Kazuhiko,
See the below table for the register difference between these two devices. No difference between LP87561IRNFRQ1 and P87561IRNFRQ1 other than the part without L is preproduction material.
LP875610RNFRQ1 | LP87561IRNFRQ1 | ||||
Register address | Bitfield name | Value | Value description | Value | Value description |
0x01 | OTP_ID | 0x10 | 0x10 | 0x98 | 0x98 |
0x02 | EN_BUCK0 | 0x00 | DISABLED | 0x01 | ENABLED |
0x02 | EN_PIN_CTRL0 | 0x00 | Only EN_BUCK0 bit | 0x01 | EN_BUCK0 bit AND ENx pin |
0x03 | ILIM0 | 0x07 | 5.0 A | 0x06 | 4.5 A |
0x04 | EN_BUCK1 | 0x00 | DISABLED | 0x01 | ENABLED |
0x04 | EN_PIN_CTRL1 | 0x00 | Only EN_BUCK1 bit | 0x01 | EN_BUCK1 bit AND ENx pin |
0x05 | ILIM1 | 0x07 | 5.0 A | 0x06 | 4.5 A |
0x06 | EN_BUCK2 | 0x00 | DISABLED | 0x01 | ENABLED |
0x06 | EN_PIN_CTRL2 | 0x00 | Only EN_BUCK2 bit | 0x01 | EN_BUCK1 bit AND ENx pin |
0x07 | ILIM2 | 0x07 | 5.0 A | 0x06 | 4.5 A |
0x08 | EN_BUCK3 | 0x00 | DISABLED | 0x01 | ENABLED |
0x08 | EN_PIN_CTRL3 | 0x00 | Only EN_BUCK3 bit | 0x01 | EN_BUCK3 bit AND ENx pin |
0x09 | ILIM3 | 0x07 | 5.0 A | 0x06 | 4.5 A |
0x0A | BUCK0_VSET | 0x0A | 600 mV | 0x39 | 900 mV |
0x0C | BUCK1_VSET | 0x0A | 600 mV | 0x39 | 900 mV |
0x0E | BUCK2_VSET | 0x0A | 600 mV | 0x39 | 900 mV |
0x10 | BUCK3_VSET | 0x0A | 600 mV | 0x39 | 900 mV |
0x19 | EN3_PD | 0x01 | ENABLED | 0x00 | DISABLED |
0x19 | TDIE_WARN_LEVEL | 0x01 | 137C | 0x00 | 125C |
0x19 | EN2_PD | 0x01 | ENABLED | 0x00 | DISABLED |
0x19 | EN1_PD | 0x01 | ENABLED | 0x00 | DISABLED |
0x21 | TDIE_WARN_MASK | 0x01 | MASKED | 0x00 | UNMASKED |
0x22 | RESET_REG_MASK | 0x00 | UNMASKED | 0x01 | MASKED |
0x28 | PG3_SEL | 0x00 | Masked | 0x03 | Power-Good-threshold voltage AND current limit |
0x28 | PG2_SEL | 0x00 | Masked | 0x03 | Power-Good-threshold voltage AND current limit |
0x28 | PG1_SEL | 0x00 | Masked | 0x03 | Power-Good-threshold voltage AND current limit |
0x28 | PG0_SEL | 0x01 | Power-Good-threshold voltage | 0x03 | Power-Good-threshold voltage AND current limit |
0x29 | PGOOD_WINDOW | 0x01 | Overvoltage and undervoltage monitoring | 0x00 | Only undervoltage monitoring |
0x2C | EN_SPREAD_SPEC | 0x00 | DISABLED | 0x01 | ENABLED |
I2C address | 0x62 | 0x60 |
BR,
Samuli
Samuli,
Why preproduction material device (without L) is listed in the datasheet?
Any specific reasons?
Best regards,
K.Hirano