This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM36922: LED fails due to LM36922 default state.

Part Number: LM36922

Hi Team, 

We are using LM36922 LED driver. Due to the default state of led driver the LED got spoiled. 

Our maximum led current is about 15mA. 

If I2C fails, the led gets a maximum current from the driver. Because the default state of the driver is high. 

 

So, What shall we do for avoid this problem. Even the I2C fails driver should not deliver more than 15mA. Will you please give your suggestion for this.