Other Parts Discussed in Thread: BQSTUDIO
Hi team,
please help my customer to program BQ27520-G4:
I'm developing on board programming for their board with the device BQ27520-G4.
The customer sent us the attached programming file .srec.
It's seems to have the following memory area:
- 0x00004000 - 0x000043FF
- 0x00100000 - 0x0010FFFF
Unfortunately in the document "SLUUA35" I don't find a correlation between programming file addresses and component registers.
So I don't understand if this data needs to be programmed in the uC.
The customer seems to use that file with the TI BQ Studio tool.
These are the only commands I understand that are available for flash management:
Here below the device register I understand the uC allows to be programmed:
- Subclass ID (access using command code 0x3E)
- Subclass (access using command code 0x3F)
- Offset of various register
Please can you help me understand how the file should be used and the relation between the addresses and the memory area of the uC?