Can I connect the RST_SHUT to TS2 to create a 'system present' function. I'm thinking that when RST_SHUT is high, the device should enter shutdown, then when the line is taken low, TS2 will go low and cause the device to wake up. Will this work or is there a better way to create a single line / shutdown/wake up function?