Hi,
How to design the second stage filter for TPS54561?,
output 5.5V /5A,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
When you say second stage filter, are you referring to the input EMI filter?
If so, please refer to this app note for more details (https://www.ti.com/lit/an/snva489c/snva489c.pdf)
Depending on your level of attenuation, the Lf and Cf will need to be appropriately tuned.
Regards,
Jimmy
Hello Anoop,
for a simple rule of thumb approach, I suggest the following. Where Lbuck is the buck inductor, Lf is the filter inductor, Cout is the output capacitor for the buck power stage and Cf is the filter capacitor. Make Lf<<Lbuck and Make Cout <<Cf. Suggest Lf and Cout are an order of magnitude leass than Lbuck and Cf respectively.
Also note that the ESR of Cf will need to be equal to approximately Sqrt(Lf/Cf).
Therefore suggest the following with the example shown above. Make Lf = 100nH, make Cf = 470uF, ESR~15mR.
Also suggest recompensating to the following:
Rcomp = 28.7k
Ccomp = 10nF
Ccomp2 = 1nF
Hope this helps?
David.
Hi David,
Thank you for your reply,
We want to achieve below 1mV ripple. Can the above be helpful for this?
If you have any design documents, please share them.
Hello Anoop,
I ran some calculations/simulations and approximate with the design above you will be below 1mV of output ripple.
Hope this helps.
David.