This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62871-Q1: stacked mode

Part Number: TPS62871-Q1

Hello Ti  team,

in my design,  i use two TPS62871-Q1  in stacked mode to achieve max  18A current . my question is does  the two power rails draw  the same current(or nearly the same current ) at -40~85℃? 

i'm afraid one draw more current , for example  the load current is 14A,  one TPS62871-Q1 draw 9A and another draw only 5A .  please confirm , many thanks