This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Thanks!
Kai
Hi Kai,
1. LM7480-Q1 is our latest device which has integrated input reverse polarity protection where as LM5060 is an old device which needs additional circuitry for input reverse polarity protection.
2. Yes, you can protect the down stream circuitry by setting the OVP threshold at less than 48V.