We are using LM63615DQPWPRQ1 Step Down Voltage Converter in our design as we are using the TVS Diode of rated 24V and Vbr = 26.7 and clamping of 38.9V So during the Pulse 5b - TVS remain in the Breakdown region, and it gets on - large current is flowing and damaging itself.
So we are checking our product with TVS Diode - 33V rated, Vbr=36.7 and clamping voltage of 53.3, So in this case Pulse 5b - 35V time -400ms is directly applied it to LM63615DQPWPRQ1 which is having the voltage range of 3.6V to 36V. So can this IC Sustain the Pulse 5b ?
Please check on the Priority.
Kind Regards,
Shubham