This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895M: BQ25895M DSEL D+ D- pin configuration.

Part Number: BQ25895M

Hi,

I am using BQ25895M with a generic 5V Vbus input source and not a USB 5V input source.

How do I connect D+ D- and DSEL pins?

I am not using any USB handshake protocol as it is not a USB charger I am plugging into Vbus. It is a regular DC-DC switching regulator set to 5V output connected to Vbus input.

Should I leave them open/floating or do I need to connect them anywhere?

Thanks,

Srishtik.