This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: pmp10749 boost converter with dual phase

Part Number: LM5122
Other Parts Discussed in Thread: PMP10749,

Hi! I need to design a boost convert the specs with 

Application Field                               : Cold Crank (start stop)

Required  Specs for the application : In case of cold crank, the input voltage can drop to 3 volts.So  3 volt and higher input voltage value is required in accordance with this situation.

                                                           Vout: 10V output and up to 20A.

I'm trying to create a boost converter with the requirements I mentioned above. I realized that the boost converter in the design of the pmp10749 fits my requirements, However, its 10Amp output is insufficient, so I need a dual phase design. However, I don't know exactly what changes I need to make. How should I connect the syncout pin? ? Do I need to make any changes to the compensation elements? Do I need a change in the capacitor connected to the bst pin?

or other elements ?