Other Parts Discussed in Thread: TPS40428, TPSM846C24, TPS544C25, TPS549A20, TPS82150, TPS53676
Dear Sir/Madam,
I try to access TIDA-01419 - 4 Phase, 150 A Reference Design for Intel Arria 10 GX FPGAs using TPS53647 but i get this lost link error. is this reference design being update at the moment?
I am using two Intel Arria 10 GX devices in 10AX066xx and need advice on the power tree. Below is my spec and my selection:
Manufacturers Part no. |
Signal names |
Vin |
Vout |
Iout |
Max. Iout for IC's |
Group |
Type |
TPS53647 |
TPS53647_VCC |
4.5V - 14V |
0.9V |
105A , 5.12A |
240A , 40A |
G1 |
Controller |
TPS40428 |
TPS40428_VCCERAM |
|
|
|
|
|
|
TPSM846C24 (or) TPS544C25 |
TPSM846C24_VCCRT (or) TPS544C25_VCCRT |
4.5V - 15V |
1.03V |
16.27A |
35A (C24) , 30A (C25) |
G2 |
Module or Converter |
TPS549A20 |
TPS549A20(Converter)_VCCPT |
4.5V - 20V |
1.8V |
10.23A |
15A |
G3 |
Converter |
TPS82150 |
TPS82150_VCCIO_1.2V |
4.5V - 16V |
1.2V |
1A |
1A |
|
Module |
|
TPS82150_VCCIO_1.8V |
|
1.8V |
|
|
|
Module |
Do you have any advice if i have selected the best devices and any suggestion will be appreciated. thx
Best regards,
Felix