Other Parts Discussed in Thread: PMP4484
Hi team,
Can UCC28810 regulate and maintain constant voltage when the output shares with Audio amp's power supply?
My customer would like to use UCC28810 to supply LED(5W) and Audio Amp supply voltage(6~7W) at the same time. Since the current is dynamically changing depending on the Audio signal, they concerned if UCC28810 can support stable regulation voltage for LEDs. Please refer to below diagram. Customer will use base on PMP4484 reference design. The output will be single rail. So they will add an extra DCDC converter for further voltage regulation.
output voltage:
1.LED Driver: 19~23V
2.Audio AMP: 5V
Thanks,
Jay