This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866S-Q1: 14 LED in series

Part Number: LP8866S-Q1

Dear expert,

I want to use LP8866S to support 14 LED  in series. 3.3V for each LED. 14*3.3=46.2V

Max boost output of LP8866s is 48V

Is it any risk to support this scenario?

If only support 13 such kind of LED, it should be safe enough , right?