Other Parts Discussed in Thread: BQ24075, TPS61092, BQ24074,
Hi Team,
Good day! This is posted in behalf of the customer. Please see whole inquiry below.
I am trying to build a solar charger using BQ24075 EVM. I am connecting a 6V/10W solar panel at the input, a 3.7 V/1100 mAh LiPoly battery at the battery terminal and a 5 V USB device (Amazon Kindle Fire) at the output.
I have set EN1 and EN2 such that the input current is limited to 500 mA. I have disabled the timers.
With these connections, I was expecting most of the energy to be diverted to the USB device on priority and only residual energy to be used for battery charging. What I see is exactly opposite. I see the RED LED ON meaning battery is charging and the USB device shows it is not charging at all. I monitored OUT = 4.5 V and V_iset = 0.65 V.
Next, I connected CEz to Vss to disable battery charging. In this case, RED LED went OFF and the USB device started charging - but very very slowly.
I was wondering if it is something to do with the output capability of the solar panel. So I removed it and connected a wall adaptor with 5V/3A rating. The observation with CEz = HI was exactly same. The USB device charged a bit faster when CEz = VSS.
If I remove the input source, I see OUT = BAT = 3.5V and the USB device does not charge
What could be the issue?
I was suspecting if the output voltage in each case was too small to charge a USB device?
For my use case, is BQ24074 (with VOUT = 4.4 V) followed by a boost like TPS61092 a better option?
Thank you in advance!
Best regards,
Jonathan