Dear,
In TPS65381A-Q1 datasheet, VDD6 maximum output current is 1.5A, which is the load current from VDD5, VDD3/5, VDD1 and VSOUT1 on VDD6 regulator. And Peak current out of SDN6 pin is 2.5A.
But If I use VDD6 to power a load directly, how larger the output current it can offer? If the maximum load current is 2.5A, adding 1.5A from VDD5 etc., the output current from VDD6 is 4A. Can we use TPS65381 for this kind of application?
If VDD6 can power 4A load, if there is a potential risk of triggering Over-temp protection?
Thanks
BRs
Kian Lin.