Other Parts Discussed in Thread: TPS54561
Hi TI
I want to know,
1, refer from the related thread, is it right for the calculation of RUV1 with the following equation from the datasheet?
RUV1=1.215V*( RUV2/( VIN(min) +5uA*RUV2 -1.215V ) )
2, "For the design example, RUV2 = 102 kΩ and RUV1 = 21 kΩ for a shut-down voltage of 6.6 V." from the LM5116 datasheet 8.2.2.12 UVLO Divider
if RUV2=102k, then RUV1 should be RUV1=1.215V*( 102k/( 6.6V - 5uA*102k - 1.215V ) ) = 25.421k, we can use the approximate 25.5k stand value, not the 21k.
Which one is correct?
3, in 8.2.2.12 UVLO Divider, the VIN(max) is same as VIN(start) from TPS54561 datasheet equation (3) (4)? and the VIN(min) is same as VIN(stop)?