TPS62135 does not have a macro model in TINA as of yet. I tried updating already, still does not show. I then went to Tools - New Macro Wizard and followed the steps. When I got to the Shape window to select the symbol I used the default auto shape. When I do that it says that the part is invalid. See below. When I click the OK I get the next window. See below. I didn't think getting a shape from the library would work since it lists devices that are in TINA and are probably not exactly the same as this device. How can I fix this so I can use this in TINA to check out my design?