Hello:
Wondering if it is possible to inject the small signal while setting up an SMPS for loop gain-phase measurement with a nonisolated opamp for its broadband properties but of course, the limiting factor is the output common mode properties of the opamp.Pl see the circuit attached. Output DC CMC is never discussed in any Specification/data sheet.
Another hurdle is Network Analyzer such as HP 8751A( only NA we have) to be able to support Vout at Ch1 and Ch2. But that can be passed through a divider. So it is not a show-stopper.
Any review and suggestions for the Diff Opamp will be highly appreciated. It could be a current-feedback amp as well.
-r