This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] LP8756x-Q1 and LP8752x-Q1 package height

Other Parts Discussed in Thread: LP87563-Q1, LP87523-Q1, LP87565-Q1, LP87524-Q1, LP87525-Q1, LP87562-Q1, LP875701-Q1, LP87564-Q1, LP87521-Q1, LP875761-Q1, LP87522-Q1, LP87561-Q1

For LP875xx-Q1 based devices (LP87561-Q1, LP87562-Q1, LP87563-Q1, LP87564-Q1, LP87565-Q1, LP87521-Q1, LP87522-Q1, LP87523-Q1, LP87524-Q1, LP87525-Q1, LP875701-Q1, LP875761-Q1) the package height is 

  • Minimum = 0.8 mm
  • Maximum = 0.9 mm
  • Typical = 0.85 mm

Only maximum height is shown in the datasheet.