Other Parts Discussed in Thread: BQSTUDIO, , GPCCHEM
Hello,
We have a new 3000 mAh battery.
According to the datasheet of the battery, it is a li-ion battery and the charge voltage is 4.2 V, discharge voltage is 3.0 V.
For decide the chemID of this battery, we charge it until current < 30 mA, relax, and discharge with a current from 412 mA to 295 mA.
The report from TI GPC tool says the best chemID is 2530, and the max DOD error is 1.23%.
But in bqStudio, we found that ChemID 2530 is a 4.35 V LiMn2O4 battery.
The record we uploaded to GPC tool are attached below.
We programmed this ChemID 2530 to bq27520g4, and then do the learning cycle, but the learning never finish. We discharge the battery to 3.0 V, relax for 5 hours, than charge the battery to 4.2 V. But both Update Status 0/1 is still 00, not become 01.
We wonder if this (the learning cycle cannot finish) is due to the 4.35 V ChemID. Or if there is any mistake in our learning cycle process.
The following figure are voltage and current during learning cycle.
The data memory before learning cycle, and the record of learning cycle are attached below.
data_memory_before_learning.gg.csv
Thanks for your help.
Benjamin Kao