Hello,
I am designing a Flyback Transformer similar as the data sheet provided by webench for LM5023 controller IC.
In that datasheet I have a doubt about the AWG selection of the secondary winding of transformer.
The rating of the flyback converter is 19V, 3.43A at output side. That's why I think the secondary winding's wire have sufficient current carrying capacity to conduct that much of current.
But in the data sheet provided by webench they are using 2 strands of 25AWG wire. The current carrying capacity of 25AWG wire is 0.457A. Hence the total current carrying capacity will become 2 times 0.457A i.e. 0.914A which is very much lower than 3.43A.
Could you please help me to explain how this gauge selection (25AWG) is made?
Attachments:
Data Sheet of Transformer:B66423G0000X187.pdf
AWG Chart: American Wire Gauge Conductor Size Table.pdf
Also, If I will select the AWG with the current rating equal to or more than 3.43A, then the winding will unable to fit inside the above mentioned transformer core.