Hi team,
My customer tested a 2A current when the circuit is shorted. The waveforms are attached. Does this current damage the device or affect the device reliability?


Best Regards,
Peter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Peter,
Is the attached waveform showing a simulated expected normal operating condition, or is the repeated short-circuiting just a test setup?
In general this 2-A peak current won't damage the device. However, if the short-circuit event was repeatedly applied as in the attached waveform, there would be repeated temperature fluctuations, and I would expect that over time it could impact device reliability. If the short-circuit is only a fault condition and not a normal condition then this large peak current is not an issue.
Regards,
Nick
Hi Nick,
My customer saw this waveform when the device runs in normal operating condition. They are still finding the reason.
Regards,
Peter
Hi Peter,
The reason they are seeing a current spike that is larger than the current limit for this device is that the current limit circuit takes a finite amount of time to respond and limit the current. This is normal for many devices.
To clarify, what I meant in my first comment is that in the attached waveform, there is a periodic short-circuit applied to the output of the device, and if the operating conditions in their application do not have a periodic short-circuit (I would expect that they don't have a periodic short-circuit because this is a fault condition), this is not an issue from the perspective of the LDO.
Regards,
Nick