Hi there,
customer need to know the input and output frequency range of UCC21225A.
what is the max and min frequency?
BRs,
Shubiao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
customer need to know the input and output frequency range of UCC21225A.
what is the max and min frequency?
BRs,
Shubiao
Hi, Shubiao,
There is not a direct answer to that question.
The maximum switching frequency is limited by the power dissipation resulting from the capacitive load, series gate resistor, frequency, and operating voltage. The datasheet has information on how to calculate the power dissipation, and as long as it is below the maximum power handling of the device, then that combination may be used.
If the power supply is provided, the device can operate down to dc.
Best regards,
Don