This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV707: Reverse current protection

Part Number: TLV707
Other Parts Discussed in Thread: TPS7A20

Hello support team,

Customer ask if TLV707 has internal Reverse current protection between VIN and VOUT, because of abs max VOUT spec on datasheet. I assume that TLV707 has no reverse current protection, because internal block diagram shows internal parasitic diode. Is this TYPO?

TLV707

Customer point out that TLV707 should use description like TPS7A20 if TYPO. Or does TLV707 have any specific reason for the description?

TPS7A20

Thanks,

Koji Ikeda

  • Hi Ikeda-san,

    TLV707 does not have internal reverse current protection, so a VOUT max similar to the TPS7A20 would be appropriate. I don't know why it was listed this way, but if I had to guess I would think that it is because TLV707 was released in 2011 and the specifications are always improving to be more clearly defined. I'll make a note to update it.

    Regards,

    Nick