Dear Sir/Madam,
I design a power supply with Vin=70V and Vout settable by control unit to fixed values 5V, 12V, 24V, 36V, 48V and 65V. I've generated separate designs with WEBENCH for all Vout voltages and compared BOMs. The biggest differences are in FB drive voltage and Rt resistor so I decided to control these two values. My question is about control Rt resistance. I used a resistor divider (see attachment) when Rt (R112) is constant 768k (at 65V) and want to regulate voltage at RT pin by connect a "bottom" resistors to GND (R107 to R111). So is there an equation to calculate voltages at RT like those presented on Figure 8 of datasheet? Alternatively I need an internal resistance value of RT pin to calculate bottom resistors values to achieve constant Ton time with variable output voltages.
How do You think, do other components should be changed with Vout change?