Hello guys,
One of my customers is considering using TPS27SA08C for their new products.
They have the following question. Could you please give me your reply for them?
Q. We want to limit the output current less than 4A. Is the following procedure no problem?
1. Monitor SNS terminal input current with load current monitor mode (EN = H, DIA_EN = H, SEL1 = L, SEL2 = L).
2. When the output current is exceeds 4A, change EN level from "H" to "L".
3. Wait a few ms.
4. Change EN level from "L" to "H".
5. go back to No.1.
Your reply would be much appreciated.
Best regards,
Kazuya..