Other Parts Discussed in Thread: BQ24073, BQ24075, BQ25180, BQ24072
We are currently in phase of designing a new IoT product for measuring accurately Temperature and Humidity and report them in our back end. Our same previous product uses a non rechargeable battery so there is not any need for dedicate IC for recharging and dynamically change path for powering system.
We persuaded your evaluation board of BQ42073 and we are trying to configure it to meet our needs.
Some questions:
1. We want in final product to monitor battery level in order to report/alarm in case of low battery. There is a product of that series that system output follows battery level + some millivolts. What about BQ42073 which provides 4.4V out. At what voltage and above of actually battery level 4.4V remains? Is it ok to put a divider at battery input with a mosfet as a switch and measure battery voltage level at some times?
2. Can you use this IC to charge/recharge one pack of two in parallel 15650. The actual pack includes protected circuit for OverVoltage, UnderVoltage and Temperature levels.
3. What is the minimum current that this IC consumes when it is active and standby mode?
4. We want to configure IC in stand alone configuration.
Thank you in advance
Best Regard
Yannis