Other Parts Discussed in Thread: TPS536C7
Dear Team,
I'm looking to purchase the TPS536C7EVM-051 to power some demanding loads. Before doing so, I want to check a few of the board's capabilities with you:
- Can the output be set to the full 0.25-5.5V capability of the TPS536C7? I checked in the fusion GUI, but the VOUT_COMMAND seems limited to 3.739V. Can this be modified once the board is connected?
- Can the loop be made stable with the digital internal adjustments for the entire Vout span?
- Are there known limits of the switching speed on this specific evaluation board? We want to try and optimize this setup for fastest output bandwidth. Efficiency is at this moment not a huge concern.
- Is there more known about a cooling solution for this board? The manual mentions pointing a fan to keep below the advised 115C maximum. For our extended tests this does not seem like a comfortable operating temperature. Has TI experimented with other cooling solutions?
- Is there a maximum input current for this particular board? At higher output voltages this might be a constraint?
- Should I buy the usb to gpio V1 or V2 adapter? I read in other forum posts that the supported software for both usb adapters differs
Thanks for looking into this matter.
Kind regards,
Thijs