Part Number: BQ25700A
Hello TI
In my application host controller is turned on afterward by the user, first charger IC has turned on alone when the main powerline
We require to charge the battery with 500mA current initially but we can see that Charge Current Register setting resets - 0x14: 0x0000. (when main supply is removed & battery is still present)
But we can see that other resisters which we are setting i.e... 0x15 (Charge Voltage Limit), 0x3D (Input voltage Limit), and other resisters like (0x12;0x09;0x30;0x31;0x32) retain their value
1) Is there any method so that the 0x14 resistor can retain its value after restart?
2) Is there any way of connecting, with which we can power the IC from the battery so that it won't lose any register data? (Currently, we have followed Eval kit design)
Thanks
Atharv