This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160A: Whether input and output ceramic capacitors need to be placed

Part Number: TPS54160A

Hi, 

C80: Ceramic capacitor (_3225, 80V, 4.7uF, ±10%) and C6: Ceramic capacitor (_1608, 50V, 1uF, ±10%) We are investigating whether it is possible to remove two parts.

Before and after removing the parts, the following checks were carried out, and there were no particular problems.
・Check if there are any differences in ripples and spikes → No large differences
・Noise-related test → No problem

Therefore, we are proceeding in the direction of not implementing C80 and C6, but is it possible to get your opinion just in case?

Thanks,

Eevee