This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24250: Safety timer 2X period

Part Number: BQ24250

Hi team,

I've understood the default value of safety timer is not 6h but 9h by original E2E post.(Datasheet still has the typo)

My customer has one question. Which period of charging is affected from 2XTMR_EN?

Datasheet P29 "9.3.12 Safety Timer" section says "Pre-Charge or libnear mode(minimum system voltage mode" so, it means orange box in below image.

But, Datasheet P38 register map foot note says "if a condition occurs where the charging current is reduced" so, it means green box in below image.

Actual test result from customer is fit with green box.

Regards,