Other Parts Discussed in Thread: TPS43060EVM-199
Using Webench, I've created a pair of power supply circuits. One boosts 24VDC to 32VDC, the other boosts 24VDC to 40VDC. Obviously with same controllers and similar voltages many of the components are the same. The design is intended to output a maximum of 3A at each voltage.
The use of these two power supplies is to drive a single circuit - the load will be switched between them so only one voltage will be active at any given time. The "standard" voltage will be 40VDC - it will switch to 32VDC for up to 20ms and back to 40VDC for pulse signaling.
My question - is it possible to combine these two into one power supply to reduce component count and board space?