Part Number: BQ20Z95
Hi Community Members,
We use bq20z95 in our project. SBS commands return us correct values. However, extended sbs commands do not return correct values.
We tried to check which mode the bq20z95 is in with "OperationStatus (0x54)". However, this extended sbs command does not return a correct value either. In addition, we have tested 4 different batteries. The extended sbs commands for these batteries do not return correct values either.
Our questions are:
1) Could the reason why the extended sbs commands do not return correct values may be because the bq20z95 is not in the correct mode (Full Access, Unsealed, Sealed)?
2) If so, how can we check which mode the bq20z95 is in and how can we change the mode?
Thank you very much.
Best Regards.