Other Parts Discussed in Thread: TPS54202
I am using the TPS54202HDDCR for a 24V to 5V (0.5A) regulator. The 24V comes from an isolated regulator and it has a difficult time coming up if the 5V comes up before it so we have added a 1uF capacitor to the EN of the TPS54202. We have seen field failures where the EN pin becomes only about 0.8V over time and it looks to be due to mechanical stress on the cap but I want to make sure that this isn't something to do with the TPS54202 current source or something else internal not being able to handle that much capacitance on the enable. I attached our regulator circuit. Thank you in advance for the support.