Hi Expert
the Vol=3V, the describe of switch disabled protection as below:
I don't know why Vout exceed Vol when switch disabled. because Vol just 3v but Vout=vbat more than 3v.
also, how to enable 1Mohm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert
the Vol=3V, the describe of switch disabled protection as below:
I don't know why Vout exceed Vol when switch disabled. because Vol just 3v but Vout=vbat more than 3v.
also, how to enable 1Mohm?
Meng,
For the HB series, the 1MΩ resistor is always present as it is internal. There is no way to disable it. The idea is that during the off-state with the 1MΩ internal pull-up there, if there is no open load or short to battery then the current actually going to the load through such a large resistance is negligible (in the microamp range). Most, if not all of the voltage will be dropped over the internal pull-up so you won't see a significant voltage on the output.
If there is an open load or short-to-battery, essentially the only current path available is through the open-load detection circuit. In this case, the output voltage is going to be very close to the source voltage and the open load detection is going to trigger.
Timothy Logan
Applications Manager - Power Switches