This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good day,
We are using the LM5109 driver solution in interleaved buck converter design (see attached schematic). We used TIDA-010042 as a reference, just FYI.
Apart from the buck operation we also need to provide a direct path between input and output without any switching, basically a straight conductor connection. I'd like to know if it's possible to set FETs in a constant open/close mode by setting LM5109 control pins to a HIGH/LOW state for a long time (like hours), not switching as PWM? Does it seem like bootstrapping is an issue in this case? If yes - what would be the solution for us in this case, maybe another drop replacement driver or circuit modification?
Thank you in advance.
1447.Schematic.PDF
Hi Max,
Thank you for reaching out and sharing the image of the schematic! Once Vin has approached Vout, you will want to turn on both high-side switches. With both switches pulled high, you will have a constant output of Vin = Vout, and there should be no switching. This is because the output directly follows the input, so the output will be a constant high signal. To achieve this with 100% duty cycle, you will need an external charge pump (or some form of floating power supply) to help with charging the bootstrap occasionally.
I hope this answers your question! Please let me know if you have any other questions or would like more clarification.
Best,
Alex Weaver