Our design requires a total of 300uF ceramic output capacitors (6.3V caps) split between DRAMS, a CPU 1.1V supply and a few other components.
Table 8.3 indicates a maximum of 142uF, can 300uF be used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Our design requires a total of 300uF ceramic output capacitors (6.3V caps) split between DRAMS, a CPU 1.1V supply and a few other components.
Table 8.3 indicates a maximum of 142uF, can 300uF be used?
Hi steve
could you share the table 8.3? I would like to confirm if the 142uf caps for TPS65296 output?
xueliang
Hi Steve,
Yes, 300uF Output Capacitors can be used. But we tested in the lab and found that the bandwidth will be reduced by about half (130kHz -> 71kHz), so it is recommended that customers actually test Load Transient and Ripple after the modified.
Best Wishes,
Zhou
Hi steve
Using 300uF is okay, the bandwidth and phase margin depend on L*C, if customers use the 300uF, recommend using a smaller inductor of 0.33uH and actually test it on board.
xueliang