This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63050: TPS63050YFFR_High Resistor Value at the ENABLE Pin

Part Number: TPS63050

Hello,

Below is a snapshot from a schematics page, I highlighted a resistor of 2 Mega Ohm value as a part of RC circuit for power stretch application, I did that because I need the EN pin to stay HIGH for 2 minutes after the processor signal become LOW. I tested this topology, and it seems to work fine with the TPS63050YFFR, but I still have concerns regarding the 2 Mega Ohm resistor connected to the EN pin, so I need an engineer from TI to let me know if that practice is ok or not and why.