This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: EEP_ADCLOWSUPTH Value

Part Number: TPS929120-Q1
Other Parts Discussed in Thread: TPS929121-Q1,

Hi, Team

Hope you are doing well!

My customer has two questions about our TPS929121-Q1, please kindly help to explain.

1. Customer knows that the only difference between TPS929120-Q1 and TPS929121-Q1 is the V(ADCLOWSUPTH) set by CONF_ADCLOWSUPTH.

My customer is the head lighting ECU supplier. If the lighting board supplier mixes TPS929120-Q1 and TPS929121-Q1, can the MCU distinguish the two chips through software?

2. In the TPS929121-Q1 datasheet, the CONF_ADCLOWSUPTH can set threshold from 10V to 40V.

But the EEP_ADCLOWSUPTH only can set the threshold from 5V to 20V. Is there something wrong here?

Thanks & Best Regards

Jeff