This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54427: Load Transient simulation not allowing changes to load current - Webench

Part Number: TPS54427

TPS54427 support,

I tried simulating a load transient with TPS54427, and it doesn't allow any change to the load current.  It seems to fixed at 10% to 100%.  

If you open the settings for the load, you'll see () instead of "I1" and "I2".  The values are empty.  When you enter values, they aren't stored.

Is this something that can be fixed for the TPS54427 or in Webench?

I noticed a similar comment here:

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1182950/tps54622-ep-iout-setting-of-load-transient-cannot-be-done-in-webench

Thanks,
Darren