{ANS} For a number of our most popular QML Class-V radiation-hardened ceramic packaged devices (denoted with the -SP at the end of the part number) TI does offer engineering model ”/EM” versions and if these /EM parts are available you can find these orderable part numbers in the device specific product folders on ti.com, the engineering model orderable part numbers end in either /EM or -MPR. See the following link for description of the test differences between an engineering model (/EM) and full QML Class-V qualified device. Note the /EM and -MPR devices are intended for use in electrical checkout only and are not recommended in actual flight. Customers can request a limited number of samples of the /EM devices via ti.com and the sample request form can be found in the ordering and quality section of the product folders.
For our QML Class-P radiation-hardened plastic encapsulated devices (denoted with the -SP at the end of the part number) TI does not offer engineering model ”/EM” versions however we suggest that customers to use the radiation-tolerant -SEP versions of the devices for electrical checkout.
For our radiation-tolerant -SEP plastic encapsulated devices TI does not offer engineering model ”/EM” versions. Customers can request a limited number of samples of the -SEP devices via ti.com. The sample request form can be found in the "Ordering & quality" section of the product folders.